STM32WLE5 write locked not in read after passing RDP from Level 1 to Level 0
Hello,
I use STM32WLE5 on a seed studio module LORA-E5 mini where boot0 is not accessible (completely crazy ...). The module comes with a read protection and they ask us to remove RDP (level 1 to level 0) to be able to flash it with a custom program.
I was able to pass RDP from 0xBB to 0xAA in hotplug mode, all was ok exept that I cannot now erase or flash anything. I can connect in normal mode at any speed, read option bytes but no flashing. Sometimes I can erase one page but it is random ?
V target is 3.16V
stlink v2 firmware : V3j37S7
Masse erase output :
10:15:43:555 : MASS ERASE ...
10:15:43:555 : Flash erase...
10:15:43:558 : halt ap 0
10:15:43:558 : w ap 0 reg 15 PC (0x20000000)
10:15:43:559 : w ap 0 reg 17 MSP (0x20000500)
10:15:43:561 : w ap 0 reg 16 xPSR (0x01000000)
10:15:43:568 : w ap 0 @0x20001380 0x00000200 bytes Data 0x00000000
10:15:43:568 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
10:15:43:607 : w ap 0 @0x20000004 0x00000F54 bytes Data 0x0001B510
10:15:43:607 : Init flashloader...
10:15:43:609 : halt ap 0
10:15:43:610 : w ap 0 reg 0 R0 0x00000001
10:15:43:610 : w ap 0 reg 1 R1 0x00000000
10:15:43:610 : Loader mass erase...
10:15:43:610 : Error: Mass erase operation failed.Please verify flash protection
Page erase output :
10:16:50:708 : Flash sector erase ...
10:16:50:710 : Flash erase...
10:16:50:712 : halt ap 0
10:16:50:712 : w ap 0 reg 15 PC (0x20000000)
10:16:50:713 : w ap 0 reg 17 MSP (0x20000500)
10:16:50:714 : w ap 0 reg 16 xPSR (0x01000000)
10:16:50:724 : w ap 0 @0x20001380 0x00000200 bytes Data 0x00000000
10:16:50:724 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
10:16:50:763 : w ap 0 @0x20000004 0x00000F54 bytes Data 0x0001B510
10:16:50:764 : Init flashloader...
10:16:50:766 : halt ap 0
10:16:50:767 : w ap 0 reg 0 R0 0x00000001
10:16:50:768 : w ap 0 reg 1 R1 0x00000000
10:16:50:769 : w ap 0 reg 2 R2 0x00000000
10:16:50:769 : w ap 0 reg 3 R3 0x00000000
10:16:50:770 : w ap 0 reg 4 R4 0x00000000
10:16:50:772 : w ap 0 reg 5 R5 0x00000000
10:16:50:773 : w ap 0 reg 6 R6 0x00000000
10:16:50:774 : w ap 0 reg 7 R7 0x00000000
10:16:50:774 : w ap 0 reg 8 R8 0x00000000
10:16:50:774 : w ap 0 reg 9 R9 0x00000000
10:16:50:774 : w ap 0 reg 10 R10 0x00000000
10:16:50:775 : w ap 0 reg 11 R11 0x00000000
10:16:50:776 : w ap 0 reg 12 R12 0x00000000
10:16:50:776 : w ap 0 reg 13 SP 0x00000000
10:16:50:777 : w ap 0 reg 14 LR 0x20000001
10:16:50:778 : w ap 0 reg 15 PC 0x2000002F
10:16:50:779 : w ap 0 reg 16 xPSR 0x01000000
10:16:50:780 : w ap 0 reg 17 MSP 0x20001354
10:16:50:780 : w ap 0 reg 18 PSP 0x00000000
10:16:50:780 : run ap 0
10:16:50:780 : halt ap 0
10:16:50:781 : r ap 0 reg 0 R0 0x00000001
10:16:50:781 : Loader sector erase...
10:16:50:784 : w ap 0 reg 0 R0 0x08000000
10:16:50:785 : w ap 0 reg 1 R1 0x08000000
10:16:50:785 : w ap 0 reg 2 R2 0x00000002
10:16:50:786 : w ap 0 reg 3 R3 0x00000000
10:16:50:786 : w ap 0 reg 4 R4 0x00000000
10:16:50:786 : Error: Sector erase operation has failed at least for one of the existing specified sectors.Please verify flash memory protection.
Thanks for your help.
Laurent