Skip to main content
SPati.7
Associate III
March 25, 2022
Question

While transferring image from Y-Modem protocol on SBSFU, Download is aborting said that user got aborted. I am using NUCLEO-STM32H753ZI example with 2 image source.

  • March 25, 2022
  • 7 replies
  • 1319 views

=================== Main Menu ============================

 Download a new Fw Image ------------------------------- 1

 Test Protections -------------------------------------- 2

 Test SE User Code ------------------------------------- 3

 Multiple download ------------------------------------- 4

 Validate a FW Image------------------------------------ 5

 Selection :

================ New Fw Download =========================

 -- Send Firmware

 -- -- Erasing download area ...

 -- -- File> Transfer> YMODEM> Send .

 -- -- !!Aborted by user!!

 -- !!Operation failed!!

This topic has been closed for replies.

7 replies

SPati.7
SPati.7Author
Associate III
March 25, 2022

@Jocelyn RICARD​  Can you please respond to this.

SPati.7
SPati.7Author
Associate III
March 25, 2022

0693W00000Lvj9uQAB.png

Jocelyn RICARD
ST Employee
March 25, 2022

Hello @SPati.7​ ,

Apparently something goes wrong during Ymodem transfer.

Did you change anything to the original example?

Is this something new ?

Did you try erasing the full flash and check again ?

Best regards

Jocelyn

SPati.7
SPati.7Author
Associate III
March 25, 2022

Nothing i changed on example @Jocelyn RICARD​

I have just built it, and flash on NUCLO-STM32H753ZI board after Full Flash Erase.

After that i tried to enter in Download Image option on Console Terminal & Transfer File from Y-Modem option, then transferred something and Aborted.

I am using example from C:\PumpStage_POC\STM32CubeExpansion_SBSFU_V2.6.0\Projects\NUCLEO-H753ZI

Do you want me to Erase Flash again and perform ..??

if it is, can i connect programmer again ..?? do i need to do some settings ...??

Jocelyn RICARD
ST Employee
March 25, 2022

Hello @SPati.7​ 

if you didn't change anything this means you have default protections activated.

You should be able to connect under reset to the target.

If you check option bytes you should have RDP level 1, WRP on SBSFU and PCROP on a small section activated.

So, you need to perform a regression. To disable PCROP you need to set start @ higher than end @.

Also, you should switch back to RDP Level 0 and change PCROP config at same time.

WRP deactivation can be done after the regression.

What is the IDE you used, I'll try to find time to check if I get same behaviour

Best regards

Jocelyn

SPati.7
SPati.7Author
Associate III
March 25, 2022

@Jocelyn RICARD​  I am using STM32CubeIDE for my development.

I use STM32CubeProgrammer to Flash the binary.

Now after i change PCROP address & Read Level to 0, i am able to transfer image from Y-MODEM protocol.

it means, Example code itself has Read level protection set to 1 ?? & PCORP Protection as well enabled ..??

So, how can i change protection in SBSFU output binary as well .?? Which source files i can modify ..??

Can you help with that

Jocelyn RICARD
ST Employee
March 25, 2022

Hello @SPati.7​ ,

OK, so issue solved :)

To understand how things work I would advice having a look to following documents available on st.com

AN2262 : Getting started with the X-CUBE-SBSFU

UM5056 : Integration guide for the X-CUBE-SBSFU

Readme files provided with example (top one + one for each project).

Anyway, you will find all protection configuration flags in app_sfu.h in 2_Images_SBSFU/SBSFU/App

Best regards

Jocelyn