Will the example for mbedtls hardware acceleration in STM32U5 be updated?
When I use mbedtls on my STM32U585 core board without enabling hardware acceleration, it works fine. However, when I follow the instructions in some posts and copy examples, such as the rsa_alt from SBSFU under STM32U5Cube, many errors appear, and it seems difficult to fix. I noticed that the mbedtls in STM32CubeU5 seems to be several versions behind. I also tried using H5 for porting, but the result is still not satisfactory. Will there be new hardware acceleration examples for STM32U585 using STM32-MW-MBEDTLS? Thank you."