Skip to main content
rongal
Associate II
December 2, 2020
Question

X-CUBE-SBSFU installation issue inconsistencies

  • December 2, 2020
  • 1 reply
  • 1196 views

When comparing installation results with contents of Security_WS_Tools_Installation.pdf, there are the following inconsistencies:

  1. Running C:\STM32SecuWS\Tools\Other\CheckEnv.bat does not complete, as it requests STM32CubeProgrammer v2.5.0, whereas STM32CubeProgrammer v2.4.0 is the version installed by the installer.
  2. When opening ZIP File, directory C:\CSTM32SecuWS\L4 only includes subdirectory STM32CubeExpansion_SBSFU_V2.4.0, but not >Scripts or >FinishedProjects
    This topic has been closed for replies.

    1 reply

    Frantz LEFRERE
    ST Employee
    December 2, 2020

    Hello Rongal,

    1) when you launch the installer it will try to install STM32CubeProgrammer v2.5.0

    STM32SecuWS-material.exe

    > STM32CubeProgrammer 2.5.0

    > STM32CubeIDE 1.4.2

    > STM32SecuWS material

    If this binary propose to install the v 2.4.0, you don't have download the package recently ( it has been updated in September).

    Then if you already have a STM32CubeProgrammer v2.4.0 , you may just need to update the path in C:\STM32SecuWS\Tools\Other\SetEnv.bat

    This is describe in the sklide 20 of the installation guide

    2 . It was the installer that will create all the C:\CSTM32SecuWS\L4 sub structure . No zip file here.

    the only zip file in this installation process is STM32CubeExpansion_SBSFU_V2.4.0.zip this one must be unzip at location C:\STM32SecuWS\L4

    I would advise to Erase the folder C:\STM32SecuWS

    and launch again the installer and check the status.

    Best regards,

    Frantz

    rongal
    rongalAuthor
    Associate II
    December 3, 2020
    Hello Franz,
    I prepared the installation as required.
    Where and how do I join the Workshop? I registered and downloaded the necessary tools and environment, but have not received any indication on how to join the Workshop itself.
    Please forward a link to me ASAP.
    Thank you,
    Ron Gal-Ezer
    Frantz LEFRERE
    ST Employee
    December 3, 2020

    You should have the link in the invitation with the material but I send it again just now.

    Talk to you soon.

    Frantz