YMODEM for SBSFU safe enough?
Hi,
I have seen, that for the bootloader with just one image, it is only possible to use the YMODEM with UART for updating the firmware with the SBSFU. Now what I'm am concerned about is, that the YMODEM seems not to be very error tolerant.
So, what further mechanisms does the SBSFU use, to verify that the firmware is not corrupted anywhere (in case the checksum of the SBSFU fails somewhere, since it is only 16bit, right)? Will the whole firmware be checked with a checksum after reception to see, if it is valid?