Skip to main content
Associate II
February 20, 2025
Solved

adding external source file to touchGFX porject

  • February 20, 2025
  • 1 reply
  • 619 views

Hi Team,

"I'm working on a TouchGFX project that was generated using the TouchGFX Designer. I need to add source files for USB functionality. I tried adding the .c and .h files to the Core/Src and Core/Inc directories, but I'm getting an error stating that the files cannot be found. How can I properly add .c and .h files to a TouchGFX project?

Also, I am highlighting the place where I want my source file in a screenshot."

usb prob.png

 

I have a folder named TCOMP that contains .c and .h files. I also tried adding this folder to my project by updating Paths and Symbols under Properties > C/C++ General, but I'm still encountering the same error. How can I correctly include these files in my project?


Thanking you in advance

Best answer by Elhem_ZAY

hello,
to add file source file .c in STM32CubeIDE you can add it manually :
- right click on USB_HOST 
- select New > File

Elhem_ZAY_0-1740063325158.png

- select "<<Advanced" and check "link to file in the file system" 

- after that you can Browse your file source  that you want 

Elhem_ZAY_2-1740063562570.png

Best regards.
Elhem.

 

1 reply

Elhem_ZAYBest answer
ST Employee
February 20, 2025

hello,
to add file source file .c in STM32CubeIDE you can add it manually :
- right click on USB_HOST 
- select New > File

Elhem_ZAY_0-1740063325158.png

- select "<<Advanced" and check "link to file in the file system" 

- after that you can Browse your file source  that you want 

Elhem_ZAY_2-1740063562570.png

Best regards.
Elhem.

 

naveenAuthor
Associate II
February 21, 2025

hello, thank you for the response. i have followed the step as you mentioned, now iam not getting error where file not found. but small issue again here.

after added that source file i been calling a function from that source to in "USBH_UserProcess", when iam doing this USB is not detecting. debugger not even crossing the break pointer, but if i removed that calling function then everything is working as expected. can you tell me whats happing here.

I Have added some screen short for your reference.
Screenshot 2025-02-21 104819.png

also i have observed one thing,

you can see those two highlighted places in my code in which case called "HOST_USER_CONNECTION",

working fine when i call the same function dummyfile() in this case, but if i call the dummyfile() function in any another case the interrupt is not triggering. can you tell me anything i been missing here.
thanking you 
Regards,
Naveen Palle.