Board turns black instead of displaying GUI
BACKROUND:
I am using TouchGFX Designer - 4.24.0
I am using the board STM32H735G-DK
This generates STM projects in STM32CubeMX V6.11.0 using STM32Cube FW_H7_V1.11.1
When I am done with touchGFX I go to STM32Cube IDE to do some scripting on the behaviors of the GUI.
When I open the .IOC file for the first time I am prompted with a message that wants me to migrate my project to STM32CubeMX V6.11.1 using STM32Cube FW_H7_V1.11.2
PROBLEM:
If I say no to the migration and I attempt to give a "job"(EX: GPIO output) to a pin then generate code it will not correctly generate code in the main.c file. A few forums talked about the main.h or gpio.c and I look into those with no luck either. If I run the program the basic GUI set up in TouchGFX appears on the screen
If I say yes it works! All the correct code is generated correctly in the main.c file. When I attempt to run the program it executes very fast and displays a black screen after it finishes executing. No error messages occur.
EXTRANOTES:
I am not extremely familiar with all of the sections of code that are edited both by touchGFX and the stmIDE. I am slowly learning attempting to use this board in an HMI context for construction job applications.
The only thing I did not fully attempt through was creating the project on the IDE and possibly porting it over to touch GFX.
I will add a link to a drop box with the zip file of both a migrated and not migrated project, both should have very similar and simple guis
These projects are purely for testing so don't feel afraid to change them if needed.
EDIT:
Same day I realized that once I bring it over to the STMIDE, then attempt to open it in touchGFX again it is "corrupted". This is for the migrated and not migrated version.