Code no longer works after upgrading to TouchGFX v4.24
Hello everyone.
I have a project that uses CubeMX, CubeIDE, TouchGFX Designer with FreeRTOS.
Everything has been working fine until i upgrade to TouchGFX version 4.24.
I was using TouchGFX version 4.23.2, no code changed and upgraded the project in CubeMX and in TouchGFX Designer.
No faults are thrown and all other tasks seem to be running as normal.
TouchGFX never makes it to the startup-screen and the the TouchGFXTask only gets called once.
The below article is all i can find to issues, im not using JPEG-decoding nor am F7 MCU...
https://support.touchgfx.com/docs/miscellaneous/known-issues#touchgfx-4-24-0
https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/x-cube-touchgfx-4-24-0-is-out/td-p/683800
Does anybody know what is causing this issue?
Hardware config:
STM32F429
LTDC: Yes (565)
DMA2D: Yes
FMC: SRAM (double buffered frame)
JPEG: No
L8: Yes
RGB Comp: No