Display and the sensor is not working simultaneously STM32F746G- Disco
I'm working with STM32F746G- Disco Board
The display and the sensor are not working simultaneously.
when the display packages are there, the data from the sensor is not coming. If the display packages are not there, the data from the sensor is readable.
I'm using the ultrasonic sensor, and the data is not getting when the display files are there.
if I'm checking the voltage of the output pin with a multimeter it is 0v when the display packages are there.
if I'm checking the voltage of the output pin with a multimeter it is 3.3 v when the display packages are not there.
Kindly clear me that whether both the display and sensor can be worked simultaneously?