DSI display is mirrored
I am working with a custom board I designed using this display(LINK) They provide init codes on the product page that I have integrated into my project but they do not provide any any porch, timing or polarity information. I first setup LTDC and the DSI host and was able to display a solid color on the display by generating a frame buffer in code and setting each pixel. I then moved on to integrating touchGFX and was also able to get that working fairly easily but the display is mirrored on the x-axis as shown here:
The display is using a ST7701s controller, I found the MADCTL register in the datasheet that I believe should be able to mirror the display but I am not getting the expected output.
Here is how I am writing to this register
HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0x36, 0x10);
And this is the output after doing so

I have verified the ability to write to this register by setting the "BGR" bit to a 1 and the display will swap the red and blue channels, I am not sure where to even start with troubleshooting this issue.