Error in flashing STM32N6570-DK with TouchGFX
Hi all,
I used STM32H7S78-DK and everything was fine: I was able to load and flash the "HVAC Iot Demo" from TouchGFX Designer at the first time and develop my application using STM32CubeIDE.
Then I bought an STM32N6570-DK and did the same procedure as before, but I was not able to flash that demo.
I can successfully generate the code inside the TouchGFX Designer (version 4.26.0) but, when I push the button "Program and run target", I get this kind of error:
Erasing memory corresponding to segment 0:
Erasing external memory sector 0
Error: failed to erase memory
Error: failed to erase memory
c:/TouchGFXProjects/STM32N6570DK/IotDemo/MyApplication/gcc/include/flash_sections_int_ext.mk:18: recipe for target '_fsblflash_' failed
make[2]: *** [_fsblflash_] Error 1
makefile_fsbl:45: recipe for target 'flash' failed
make[1]: *** [flash] Error 2
../../gcc/Makefile:8: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
Can anyone please help me?