External flash memory - External loader failure - STM32H735IGTx MX25L12833FM21-10G
- June 9, 2024
- 1 reply
- 1581 views
Hello,
I have custom board with MCU STM32H735IGTx connected via OctoSPI to QuadSPI external flash memory MX25L12833FM21-10G
In order to flash the external memory I am using external flash loader based on the template in https://github.com/STMicroelectronics/stm32-external-loader/tree/contrib
When I am running from the embedded SW application the test template (include erase, write and memory mapping) the test pass OK.
When I am running the external loader from the cube programmer the read from 0x90000000 fails
When I am running the external loader from cube IDE I get 'Erasing external memory sectors [0 23] failure
Attached external flash BSP driver mx25l128_quadspi.c , loader template Loader_Src.c and MX driver octospi.c
Help will be highly appreciated!
Best regards