Skip to main content
Associate III
July 2, 2025
Question

Failed to simulate with STM32H750ZBT6 platform

  • July 2, 2025
  • 1 reply
  • 225 views

I build a LCD driver board with STM32H750ZBT6  ,then i want to use built-in LTDC driver and SDRAM to run 480*270*16 TFT LCD panel , but touchGFX list following wrong message, where reason from ? 

 

 

 

Generate Code
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x60EA0000, RegionSize 0x310000, State 0x10000
D:\TouchGFX\4.25.0\env\MinGW\msys\1.0\bin\sh.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0
simulator/gcc/Makefile:32: recipe for target 'assets' failed
make: *** [assets] Error 1
Failed
Failed

1 reply

GaetanGodart
Technical Moderator
July 2, 2025

Hello @miker ,

 

You have an error when generating the assets but it seems to not be caused by TouchGFX but by cygwin or windows itself.

I found 2 great forum post that could help you :

 

Regards,