Feature request: smaller generated image source files (e.g. image_EXAMPLE_IMAGE.cpp)
Currently image source files take up a lot of drive space.
My image folder TouchGFX\generated\images\src is 44.5MiB on my drive.
TouchGFX projects can take up a lot of drive space as is (https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/gfxdesigner-option-to-auto-delete-touchgfx-folder-upon-exit/m-p/724758#M39655). So these files just add to it.
You could use build scripts or cmake to add data from binary files to temporary source files. But this can be quite a hassle to make it platform independent. But that would save a lot of drive space as the binary files take up less space than source files with hex constants. (Example to use OBJCOPY)
There are ways to shrink the source files. One way is to use uint64_t hex constants instead of uint8_t hex constants to reduce overhead.
Before:
LOCATION_PRAGMA("ExtFlashSection")
KEEP extern const unsigned char image_test_image[] LOCATION_ATTRIBUTE("ExtFlashSection") = { // a x b RGB565 pixels.
0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B,
0x0C, 0x0D, 0x0E, 0x0F, 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17,
0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F, ...
};
After:
header file:
template <typename... T>
constexpr std::array<uint8_t, sizeof...(T)*8> u64_array_to_u8_array(T&&... t)
{
std::array<uint8_t, sizeof...(T)*8> out{};
std::array<int64_t, sizeof...(T)> in = {t...};
for (size_t i = 0; i < sizeof...(T)*8; ++ i) {
out[i] = uint64_t(in[i/8]) >> ((7-i%8)*8);//big endian
}
return out;
}
smaller source file:
LOCATION_PRAGMA("ExtFlashSection")
KEEP extern const unsigned char image_test_image[] LOCATION_ATTRIBUTE("ExtFlashSection") = // a x b RGB565 pixels.
u64_array_to_u8_array(
0x0001020304050607,0x08090A0B0C0D0E0F,
0x1011121314151617,0x18191A1B1C1D1E1F, ...
);
Large files can easily be 50% smaller on drives this way. Especially with wider lines and without whitespace.
I don't know how this affects compression of source files.
Using base64 would work too, but that would require c++17 or c++20 and by default TouchGFX uses c++14. Also it won't compress as well in zip or in git. Here is an example of base64: https://stackoverflow.com/a/79042473/15307950