Skip to main content
Lead II
April 13, 2026
Question

Feature request TouchGFX Designer: support min=max for slider

  • April 13, 2026
  • 2 replies
  • 180 views

For our product we use sliders to set parameters in our software. Some parameters effect the range of others at runtime. Sometimes the allowable range of the values is limited to a single value. In such a case min equals max. This leads to an assert error in the simulator and undocumented behavior on the target.
We would like to see support for min=max. One way to implement it is to show the Indicator Image in the center (or left),  disable sliding, and set the value=min=max. This would simplify our firmware since we wouldn't need to handle it as a special case.
I also added the tag bug-report since undefined behavior on the target is unacceptable.

2 replies

Senior III
April 14, 2026

I workaround would be to have 3 values with the one in the middle the value you want and have the slider disabled.

Lead II
April 14, 2026

@nico23 wrote:

I workaround would be to have 3 values with the one in the middle the value you want and have the slider disabled.


Yes. But that requires code.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Senior III
April 15, 2026

well, of course... That’s how embedded works

You can even expand the slider class and have your own class that supports the min=max

That's the beauty of coding

ST Employee
April 17, 2026

Hello @unsigned_char_array.

I have passed on your request. However, I cannot guarantee that it will be changed in the future.

On the other hand, I also think this is a case where it is quite easy to create a custom implementation.

I have attached an example in which I copied the Slider.cpp file - found in touchgfx\framework\source\touchgfx\containers after generating code with TouchGFX - to the gui\src\common folder. By doing this, your copy will be used instead of the original framework instance. I made a few relatively simple modifications to support the case where the min and max values are the same, and I also implemented a small test example. Please note that I have not tested it very thoroughly.

Best regards,
Johan