Getting a Hard Fault while debugging a TouchGFX example project on STM32H757I-EVAL
Split from this thread for a new question.
Thank you. I've changed the programmer, and it now programmed without errors.
I however get a Hard Fault, sitting in HardFault_Handler(), as soon as I run. It happens before the code gets to main(). It also does not look like it is matching symbols to files correctly, because it is not showing code. I did check that Load Symbols is checked in debugger settings.
Can this HardFault be related, or should I start new post to help with that?