Skip to main content
HBalo.1
Associate
August 24, 2020
Question

hello guys. i work with touch GFX but i have a question. can i startup a 7" LCD with stm32f469i eval? if yes how?

  • August 24, 2020
  • 4 replies
  • 1238 views

and more, how the characteristic parameter this LCD has?

This topic has been closed for replies.

4 replies

Alexandre RENOUX
Visitor II
August 24, 2020

Hello,

What is this 7'' LCD ? Because it's not the one embedded on the F469-EVAL.

Please provide more information.

/Alexandre

HBalo.1
HBalo.1Author
Associate
August 30, 2020

In fact, I designed my work in touchgfx software on stm32f469 eval.

Now if I design a board exactly like the stm32f469 eval board and put a 7-inch lcd with a resolution of 480 x 800 on it, according to the touchgfx settings, will the code generated by touchgfx run on this hardware?

And my question is exactly what 7-inch LCD should I get so that I do not get into trouble?

Will the problem be solved just by changing the settings of the LTDC unit according to the 7-inch LCD?

Alexandre RENOUX
Visitor II
September 7, 2020

Hello,

Yes in theory the code generated by CubeMX and TouchGFX should work.

For the screen, we don't have any recommendation in particular. If you choose a LTDC screen, this will simplify the implementation as LTDC is fully handled by TouchGFX Generator.

/Alexandre

mehmet06
Associate
March 12, 2024

I want to use a 7 inch and above screen with toucgfx and you do not know which screen I can use. So what use will this kit be if I can't make an original design and I can't even find the screen on it? I paid a ton of money for the stm32f469 i kit.