Skip to main content
Senior II
September 10, 2024
Solved

how to integrate touchgfx and dac

  • September 10, 2024
  • 2 replies
  • 870 views

how to connect sine wave generation code to the TouchGFX interface and when a button is clicked it has to move to second page and trigger the generation ,how to use the mvp model,this the code for the sine wave generation and contiously writing to dac .

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

DAC_HandleTypeDef hdac1;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DAC1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
int time1=0;
int time2=0;
int end1=172;
int end2=141;
int max1=480;
int max2=200;
#define PI 3.1415926
/*void delay (uint16_t delay){
	__HAL_TIM_SET_COUNTER(&htim2,0);
	while (__HAL_TIM_GET_COUNTER(&htim2)<delay);
}*/
uint32_t var1;
uint32_t var2;
uint32_t value1[10000];
uint32_t value2[10000];
void get_sineval ()
{
	for (int i=0;i<end1;i++)
	{
		value1[i]=((sin(i*2*PI/end1)+1)*(max1/2));
	}
	for (int i=0;i<end2;i++)
	{
		value2[i]=((sin(i*2*PI/end2)+1)*(max2/2));
	}
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DAC1_Init();
 /* USER CODE BEGIN 2 */
 get_sineval();
 HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
 HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);
 //HAL_TIM_Base_Start(&htim2);


 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 /* USER CODE END WHILE */
	 	 var1 = value1[time1];
	 	 	 	 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, var1);
	 	 	 	 time1+=1;

	 	 	 	 if (time1>end1-1)
	 	 	 		 time1=0;
	 	 	 	 var2 = value2[time2];
	 	 	 	 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_12B_R, var2);
	 	 	 	 time2+=1;


	 	 	 	 if (time2>end2-1)
	 	 	 		 time2=0;


 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /*AXI clock gating */
 RCC->CKGAENR = 0xFFFFFFFF;

 /** Supply configuration update enable
 */
 HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 25;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief DAC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DAC1_Init(void)
{

 /* USER CODE BEGIN DAC1_Init 0 */

 /* USER CODE END DAC1_Init 0 */

 DAC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN DAC1_Init 1 */

 /* USER CODE END DAC1_Init 1 */

 /** DAC Initialization
 */
 hdac1.Instance = DAC1;
 if (HAL_DAC_Init(&hdac1) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT1 config
 */
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT2 config
 */
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC1_Init 2 */

 /* USER CODE END DAC1_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

    Best answer by mƎALLEm

    Hello,

    Based on what I suggested from your previous thread: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/sine-wave-generation-using-touchgfx/td-p/718218

    I suggest you to see this video especially how to toggle a LED by pressing a button from the GUI. You need to implement the same thing with DAC On/Off.

    Hope it helps.

     

    2 replies

    mƎALLEm
    mƎALLEmBest answer
    Technical Moderator
    September 10, 2024

    Hello,

    Based on what I suggested from your previous thread: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/sine-wave-generation-using-touchgfx/td-p/718218

    I suggest you to see this video especially how to toggle a LED by pressing a button from the GUI. You need to implement the same thing with DAC On/Off.

    Hope it helps.

     

    "To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
    GaetanGodart
    Technical Moderator
    September 11, 2024

    Hello @Sharan ,

     

    As SofLit mentioned, to communicate between the standard application (main.c) and TouchGFX, you need to use the MVP design-pattern.
    We have made a guide about it : model-view-presenter-design-pattern 
    SofLit also shared a pretty good video about how to use MVP.

    I see that you have made two post about the same issue (previous post) . It makes it harder for us to help you if you create a new post each time. I recommend we keep the discussion about using a sin wave in this post.

    I think you next steps are :

    1. watch the video 
    2. read the documentation 
    3. implement your sin wave function use what you feel the best (math.h?)
    4. propagate the sin wave value to TouchGFX through the MVP design pattern

     

    If you have another specific question about this subject, feel free to ask it in this post as a comment! 

     

    Hope this helps. :smiling_face_with_smiling_eyes:

     

    Regards,