How to remove gaps in scrollwheel list
I have a scrollwheel with cicular function working on my screen. The list is variable depending on how many pages are required on the screen. At the moment I have 3 numbers exposed to show the next and previous pages in the list. This creates 5 drawables in the Base file. If I have less than 5 pages in the list I get gaps in the list (ie Page 1, 2, 3, , ,).
I could load in the spaces with the next number but then that makes it illogical because it will then end up 1,2,3,1,2.
Can I reduce the number of drawables or is there a way to fill the gaps to keep it logically moving continuously