Skip to main content
Associate III
November 27, 2024
Solved

Migrating TouchGFX Simulator Project to STM32H7S78-DK Board

  • November 27, 2024
  • 2 replies
  • 783 views

Hello,

I am currently working with the TouchGFX Designer tool and have successfully created a simulator project. I would now like to migrate this project to the STM32H7S78-DK board but am unsure of the necessary steps or adjustments required.

Could you please guide me through the migration process?

Board: STM32H7S78-DK
TouchGFX Version: 4.21.1
IDE: STM32CubeIDE


Thank you!
Mehul

Best answer by Imen.D

Hello @Mehulrana511 

To migrate the project, you can use the "Import GUI' option in the "Edit" tab in Designer:

Click the "Import GUI" button to open the Import GUI window. Then, click the "Browse" button allowing for selection of a TouchGFX Designer project (.touchgfx) to be imported into the current project.

Please follow the steps in this TouchGFX guidelines.

2 replies

Imen.DBest answer
Technical Moderator
November 27, 2024

Hello @Mehulrana511 

To migrate the project, you can use the "Import GUI' option in the "Edit" tab in Designer:

Click the "Import GUI" button to open the Import GUI window. Then, click the "Browse" button allowing for selection of a TouchGFX Designer project (.touchgfx) to be imported into the current project.

Please follow the steps in this TouchGFX guidelines.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Associate III
December 19, 2024

Hi,
I have successfully migrant simulator project to STM32H7S78-DK board,
but after migration load and simulator option is disabled.
Here i attached screenshot,

Mehulrana511_2-1734621893012.png

 

/Mehul