NemaGFX v1.3.0 M7 (STM32H7RS) - Some limitations being worked on?
Hello STM32 enthusiasts,
While testing NemaGFX v1.3.0 for the STM32H7RS (M7), I discovered some differences compared to NemaGFX v3.5.0 for the STM32U5x9 (M33).
1. nema_clear(color); Doesn't work, I had to come up with some solution:
nema_matrix3x3_t m;
NEMA_VG_PAINT_HANDLE paint;
uint32_t color = nema_rgba(0xFF, 0xFF, 0x00, 0xFF);
/* Fill the screen with a color */
#if defined(STM32H7S7xx)
/* Use this on STM32H7RS */
paint = nema_vg_paint_create();
nema_vg_paint_clear(paint);
nema_mat3x3_load_identity(m);
nema_vg_set_fill_rule(NEMA_VG_FILL_NON_ZERO);
nema_vg_paint_set_paint_color(paint, color);
nema_vg_draw_rect(0, 0, DISPLAY_SIZE_W, DISPLAY_SIZE_H, m, paint);
nema_vg_paint_destroy(paint);
#else
/* Does not work on STM32H7RS */
nema_clear(color);
#endif2. nema_bind_src_tex / nema_blit Does not work with the NEMA_AL88 format, but luckily it does work with the NEMA_ARGB8888 format.
// Format = NEMA_AL88 /* Doesn't render any output using AL88 bitmaps */
Format = NEMA_ARGB8888 /* Works fine using ARGB8888 bitmaps */
nema_set_const_color(nema_rgba(0xFF, 0xFF, 0x00, 0xFF));
nema_set_blend_blit(nema_blending_mode(NEMA_BF_SRCALPHA, NEMA_BF_INVSRCALPHA, NEMA_BLOP_MODULATE_RGB | NEMA_BLOP_MODULATE_A));
nema_bind_src_tex(Data, Width, Height, Format, Stride, NEMA_FILTER_BL);
nema_blit(x, y)
3. Not all types of gradients work, like NEMA_VG_PAINT_GRAD_RADIAL and possible more.
float x = 400;
float y = 240;
float w = 100;
float h = w;
float w2 = w / 2;
float h2 = h / 2;
nema_vg_paint_set_type(paint, NEMA_VG_PAINT_GRAD_RADIAL);
nema_vg_paint_set_grad_radial(paint, gradient, x + w2, y + h2, w2, 0);Will these issues be fixed in a later release of NemaGFX?
Or is the GPU2D in the M7 simply not capable of this?
Or am I probably doing it wrong? (Most probably, though!)
Sincerely, Jack.