NUCLEO-WL55JC2: TouchGFX never displaying anything to screen
Hey all, I've used this tutorial: https://youtu.be/suMytEyQTP4?si=jLtyF5uH1Qd6zpYv
to run TouchGFX on several different MCUs/boards such as the black pill or NUCLEO-F446RE. However, I simply cannot get anything to display when I setup TouchGFX on my NUCLEO-WL55JC2. I'm unsure if there is something I'm missing that makes it unfeasible or much more difficult to get it running on the board, but I'm at my wit's end after debugging for hours and finding no issue. The code compiles and programs to the board fine, and I've verified all connections as well as parameters, and I am at a loss as to what to do. If anyone could help I would greatly appreciate it. (Note: I've tried in single core setup to get it to work as well and that did not seem to solve the issue.)