Partition a QSPI NOR Flash in memory mapped mode
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code or a script. Please read this post: How to insert source code.
Hi
This is something very easy that I am missing or impossible. I am using a nucleo-l476 to drive an RA8875 with a flash memory attached. This is using touch gfx to drive the RA8875 LCD. I am switching in/out of memory mapped mode to rewrite part of the flash memory so I can load different images into the flash memory and touch gfx will load the new images from the nor flash (This all works beautifully).
what I am trying to do is have touch gfx load an image to a different part of the nor flash using partitioning. see linker below.
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 96K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
QSPI_NOR (xrw) : ORIGIN = 0x90000000, LENGTH = 8M
QSPI_NOR_P (xrw) : ORIGIN = 0x90800000, LENGTH = 8M
}
/* Sections */
SECTIONS
{
ExtFlashSectionP :
{
*(ExtFlashSection ExtFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x100);
} >QSPI_NOR_P
ExtFlashSection :
{
*(ExtFlashSection ExtFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x100);
} >QSPI_NOR
FontFlashSection :
{
*(FontFlashSection FontFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x100);
} >QSPI_NOR
the issue is touch gfx wont show or allow me to write to the separate partition
on the nor flash. is what i am trying to do possible and if so what am i missing.