Problem with app.mk using relative path to TouchGFX env folder
Hi
I just noticed that when building the Simulator using TouchGFXDesigner 4.24.1 the files
/config/gcc/app.mk
and
/config/msvs/Application.props
are updated with the relative path to the TouchGFX env folder, for instance:
# Location of the TouchGFX Environment
touchgfx_env := ../../../../../TouchGFX/4.24.1/env
If I try to overwrite these paths the files are just overwritten when I run the Simulator from TouchGFX Designer.
This is a problem when working on a project with multiple people that may have the project check out at different folder depths. I don't think the solution is to require that the project is checkout out at the same folder depth for everyone on the same project.
You can argue that it isn't a big problem as TouchGFX Designer updates the path for anyone creating the Simulator.
But it does create 'noise' in the repository.
Any suggestions on how to solve this ?
//Jesper