screen tearing when using .invalidate on the STM32H735G-DK
PROBLEM:
I do not believe this is a bug. I am doing everything I can to read into this issue it seems like I am either not enabling all the correct options or I am using .invalidate wrong.
This is what my GUI looks like from a basic design.
This is what it looks like when I run the TouchGFX simulator(the right image is gone because I initialize it as false until it receives a signal)
This is the tearing image I am having trouble with(currently no inputs).

I am basing this example on a set of tutorials I found online, https://www.youtube.com/watch?v=Y7d6-59YQu8&t=525s.
At my current level of C programming he seems to provide a good amount of details. Where I fall short is once I start to run it on the board.
CODE IN QUESTION:
#include <gui/screen1_screen/Screen1View.hpp>
Screen1View::Screen1View()
{
}
void Screen1View::setupScreen()
{
Screen1ViewBase::setupScreen();
}
void Screen1View::tearDownScreen()
{
Screen1ViewBase::tearDownScreen();
}
void Screen1View::setLight(bool state)
{
Light_ON.setVisible(state);
Light_OFF.setVisible(!state);
Light_ON.invalidate();
Light_OFF.invalidate();
}
WHAT I HAVE TRIED:
-> My first impression was that I was refreshing my screen to fast. I took out the .invalidate line, the gentlemen in the tutorials described it as a way to let the system know the widgets graphical representation needs to be reset. If I did that it would stop "tearing" and stay still, no matter what input I gave in D6(PD15) which I set as my GPIO Input.
-> I created a timer which would only call .invalidate every second. This partially worked! it correctly showed my inputs were working and the images changed but alas every second before the new image showed up it would "tear". All other examples I saw of the STM32H735G-DK did not do this.
-> I looked more into invalidate. The closest I got to a proper explanation was that some boards use "Double buffer". Double buffer seems to be a way to ensure the board will not try to clear and write to the screen at the same time. I am unsure of how to find the option to start double buffering.
ENDING:
Although double buffering may not be the issue, it is my best first steps. If this does not seem plausible and you guys have other ideas on what could be causing this issue please let me know. Thank you for all of your help.
NOTE: it says "your post has changed because of invalid HTML" I apologize if the grammar is strange or missing in any areas I missed.