Scrolling text wider than the LCD screen
I am using TouchGFX Designer (version 4.24.1).
I am wanting to stroll a Text Area across the screen. I can do this with the MoveAnimator selected as long as the text width is less than the screen width. When I attempt to scroll text than is wider than the LCD screen width, then anything wider than the screen is lost.
The scrolling code being used is as follows:
txtCalibDetails.clearMoveAnimationEndedAction();
txtCalibDetails.startMoveAnimation(240, 299, 480,
touchgfx::EasingEquations::linearEaseNone,
touchgfx::EasingEquations::linearEaseOut);Please note regarding the x and y values (240, 299): I've created the screen in TouchGFX Designer upside down so that I can have then screen rotated by 180 degrees on the LCD without further processing.
How can I scroll text that is wider than the screen width?
Thanks