Solved
STM32F423ZHT6- ST7789H2
I sent a write data to LCD like display the RED background on the LCD panel. But it display like this-

this is my code part:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FSMC_Init();
MX_CRC_Init();
MX_FMPI2C1_Init();
/* USER CODE BEGIN 2 */
ST7789H2_Init();
LCD_Fill(0xF800, 0, 0, 240, 240);
/* USER CODE END 2 */
/* Init scheduler */
osKernelInitialize();
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* creation of defaultTask */
defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_EVENTS */
/* add events, ... */
/* USER CODE END RTOS_EVENTS */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void LCD_Fill(uint16_t RGBCode, uint16_t Xpos, uint16_t Ypos, uint16_t width, uint16_t height)
{
for (uint16_t i=0; i<height; i++)
{
ST7789H2_DrawHLine(RGBCode, Xpos, Ypos++, width);
}
}
#include "main.h"
#include "LCD_Controller.h"
#define FMC_BANK1_REG ((uint16_t *) 0x60000000) // Register Address for A0
#define FMC_BANK1_DATA ((uint16_t *) 0x60000002) // Data Address for A0 -> A0<<1 -> 0010
void LCD_IO_WriteReg(uint8_t Reg)
{
*FMC_BANK1_REG = Reg;
}
void LCD_IO_WriteData(uint16_t RegValue)
{
*FMC_BANK1_DATA = RegValue;
}
void LCD_IO_WriteMultipleData(uint16_t *pData, uint32_t Size)
{
for (uint32_t i=0; i<Size; i++)
{
LCD_IO_WriteData(pData[i]);
}
}
uint16_t LCD_IO_ReadData(void)
{
return *FMC_BANK1_DATA;
}
void LCD_IO_Delay(uint32_t delay)
{
HAL_Delay(delay);
}
void LCD_IO_Init(void)
{
HAL_GPIO_WritePin(MC_LCD_RESET_GPIO_Port, MC_LCD_RESET_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(LCD_ENABLE_GPIO_Port, LCD_ENABLE_Pin, GPIO_PIN_RESET);
LCD_IO_Delay(5);
// HAL_GPIO_WritePin(BL_CONTROL_GPIO_Port, BL_CONTROL_Pin, GPIO_PIN_RESET);
// LCD_IO_Delay(5);
HAL_GPIO_WritePin(MC_LCD_RESET_GPIO_Port, MC_LCD_RESET_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(LCD_ENABLE_GPIO_Port, LCD_ENABLE_Pin, GPIO_PIN_SET);
// HAL_GPIO_WritePin(BL_CONTROL_GPIO_Port, BL_CONTROL_Pin, GPIO_PIN_SET);
}
Can anyone help me?