STM32H750B-DK: Integrate LwIP Ethernet + TouchGFX + External QSPI Flash
Hi, I'm working on the STM32H750B-DK discovery board and need to combine two key functionalities:
1. Ethernet connectivity based on the LwIP stack (using the example from the `stm32-hotspot/STM32H7-LwIP-Examples` repository).
2. A TouchGFX GUI that stores its assets (images, fonts) in the external QSPI flash (`MT25TL01G`) due to the limited internal flash (128KB).
I have both components working **individually**: - The **standalone Ethernet example** (STM32H750_Disco_ETH) works perfectly – I can ping the board at `192.168.1.10`.
- The **standalone TouchGFX application** works when the external flash is properly initialized via a bootloader, and assets are loaded from `0x90200000`.
The challenge is to merge them into a single project where the application code runs from internal flash (the `APP_FLASH` region) and the Ethernet stack functions correctly alongside the TouchGFX GUI. ### **Current Memory Map (Linker Script)** I am using the following memory partition to accommodate both: `
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 8M
ASSETS_FLASH (r) : ORIGIN = 0x90200000, LENGTH = 126M
/* Partition internal flash */
BOOTLOADER (rx) : ORIGIN = 0x08000000, LENGTH = 32K /* Reserve 32KB for bootloader */
APP_FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 96K /* Remaining 96KB for app */
}### **The Problem** When I attempt to merge the two, I encounter a "Load failed" error during debugging because the debugger cannot write to the external QSPI flash at `0x90200000` without an external loader. More importantly, the Ethernet stack often fails to initialize (ping timeout) or the system hard-faults, likely due to the QSPI not being initialized early enough for code that may be inadvertently placed in external flash.
My Approach & Questions
1. **Bootloader Role:** The bootloader at `0x08000000` initializes the QSPI in memory-mapped mode and then jumps to the application at `0x08008000`. Is this the correct sequence to ensure the external flash is ready before the main application (including LwIP) starts?
2. **Linker Script Placement:** How can I ensure that **all code and initialized data for LwIP and the core application** are placed strictly in internal flash (`APP_FLASH`) and **not** in external `ASSETS_FLASH`? The `ASSETS_FLASH` region should only contain read-only GUI assets, not executable code.
3. **MPU Configuration:** The Ethernet example uses specific MPU regions for the LwIP heap (`0x30020000`, non-cacheable) and descriptors (`0x30040000`, non-cacheable, shareable). Do I need an additional MPU region for the external QSPI flash address range (e.g., `0x90000000` or `0x90200000`) to make it cacheable for performance, or will that interfere with Ethernet DMA?
4. **Debugging with External Flash:** What is the recommended workflow for debugging such a project? I have used STM32CubeProgrammer with the `MT25TL01G_STM32H750B-DISCO.stldr` loader to flash the image manually, but it breaks the seamless debug-test cycle in CubeIDE. Is there a way to configure the IDE to use the external loader automatically?
Request
Has anyone successfully integrated the `STM32H750_Disco_ETH` LwIP example with a TouchGFX project that relies on external QSPI flash? Could you share a working linker script snippet, the necessary MPU settings, and your approach to debugging?
Any guidance or examples would be immensely helpful. Thank you!