Skip to main content
Visitor II
September 30, 2025
Solved

TouchGFX 4.26.0 touch_core_libcpp

  • September 30, 2025
  • 1 reply
  • 300 views

Hi, 

I am using Touch GFX 4.26.0 and the EWARM9 compiler.
It was announced that libcpp support was available from 4.25.0 onwards.
I have confirmed that IAR9.x\touch_core_libcpp.a for cortex-m7 is supported. (STM32H7)
However, I cannot build touch_core_libcpp.a for other cores, such as cortex-m33(STM32U5).
As a temporary measure, I am using cortex-m7\IAR9.x\touch_core_libcpp.a for cortex-m33.
Could there be a mistake in the compile switch when generating the library?

I had the same issue with 4.25.0, and was hoping it would be fixed in 4.26.0, but it wasn't.

fu1429_0-1759195999525.png

エラー[Li009]: runtime model conflict: Module Font.o(touchgfx_core_libcpp.a) specifies that '__CPP_Library' must be 'DLib', but module AnalogInThread.o has the value 'libc++'

Best answer by PeterVang

Hello,

I have just checked this issue and can see that we unfortunately (like you suggested) have made a mistake in our build setup for this library.

Thank you for making us aware of this issue. It will be fixed in the next release of TouchGFX.

Best regards,

Peter

1 reply

PeterVangBest answer
ST Employee
November 6, 2025

Hello,

I have just checked this issue and can see that we unfortunately (like you suggested) have made a mistake in our build setup for this library.

Thank you for making us aware of this issue. It will be fixed in the next release of TouchGFX.

Best regards,

Peter