TouchGFX and isomtery - isometric image
Is there any example how to create any simple animation? I would like to get object in motion using static isometric view. Object based on the few outlines of rectangles outlines with painter or putting the texture on it. I need to rotate one pseudo 3D rectangle in reference to the other. It is not so hard for 500MHz CPU, the issue comes with additional effects like lighting but it is not so important.