TouchGFX breaks SDMMC DMA transfert for FatFS using SD card
Hi,
I have a STM32F779BI on a custom board that communicates with a LCD display using the LTDC interface in 16bits (480x272). I am using a single buffer inside the RAM of the MCU. So far TouchGFX works pretty well but once i activated the Software package for touchgfx inside Cubemx, i see that a "MX_TouchGFX_Init();" is added in the Main init section and i have to manually call the "MX_TouchGFX_Process();" in a task when all my board is up and running and can finally start the drawing process on the LCD.
My problem is that i have a task for logging data on a SD card using FatFS. Since i am using FreeRTOS, i had to implement the writes and Reads using the DMA on the SDMMC. This works pretty well too when touchgfx is not initialized ("MX_TouchGFX_Init();") and started ("MX_TouchGFX_Process();").
At first i thought it was a problem of NVIC priority for the SDMMC DMA versus the DMA2D interrupt priority. However, i made sure to give the DMA2D a priority less than for the DMA SDMMC and it still don't work.
The reason i know it's not behaving correctly is that FatFs return "FR_NO_FILESYSTEM" when doing a "f_open()". Normally, the FatFs generated by CubeMx does not need any modifications and if it breaks, is usually due to a lower layer (DMA transfer in this case).
Has anyone experienced problem with the Sdcard when using touchgfx in this communiation: SDMMC+DMA+FATFS+FReeRTOS+TouchGFX?
I have provided the project as is where you can look into my cubemx file for settings.
Thanks in advance for the help.