Touchgfx: button click trigger wrong callback function
Hi Team,
Issue summary: when button is clicked then other button callback function getting trigger on TouchGFX simulation and same on hardware.
Hardware details: STM32F429 Disc1 board
TouchGFX version: 4.24.0
UI snip: When I click within area marked in square sky color box which is button area then kitchen callback function is triggered which is fine; but which also covers the 30% around area of Lobby. So when I click on Lobby button which is part of Kitchen button(around 30%) then kitchen callback function is triggered. So question is how to resolve this isseu.
TouchGFX UI screen
Thanks
MR