Touchgfx circular progress bar.
I'm using the stm32h750-dk development board and TouchGFX 4.21.4 and STM32CubeIDE. I want to design a circular progress bar with a color gradient. I attached the required circular progress bar as an image. so I want to control the circular progress bar from the main.c using an external variable resistor. I'm Using the 'queue' to communicate between touch TouchGFX files and main.c file. Still, I can control the progress bar using a single color (without a color gradient). anyone can help me to implement a circular progress bar with a color gradient when progressing the bar.

this is the code that I use now.