touchgfx compression tearing
I'm using TouchGFX version 4.24.1 with external flash memory mapping at address 0x90000000.
When using the original image, there are no issues. However, when using the compressed RGB565 function, a tearing effect appears on the LCD screen. If I disable 'SCB_EnableDCache()', the issue is resolved.
Therefore, I believe that 'TouchGFXGeneratedHal::InvalidateCache()' is not properly invalidating the decompression buffer
- Is there a solution for this?
- If I disable 'SCB_EnableDCache()', will it have a significant impact on display performance?"