TouchGFX Designer align and distribute
Hi I'm just starting to use TouchGFX designer, with a background in other UI design programs, and one thing I'm frustrated about is the lack of the ability to align and distribute assets on a screen. I do appreciate the snapping that happens but if I need to distribute a number of objects evenly or just batch align them all with one click, it becomes bit of a pain to manually type x and y locations for each one.
I guess it's not that big of a deal, but just a feature that I feel is missing from a UI design software that others have and feels like TouchGFX is behind in this aspect.
Also there is a bug in 4.25.0 where if you have multiple objects selected and then move them, when you deselect them by clicking elsewhere, the mouse automatically latches to the "box select" mode.