TouchGFX designer generates faulty code for evalboard hardware buttons
Hi,
I am playing with a G071RB evalboard + GFX01M2 display shield atm and noticed some faulty code being generated by TouchGFX designer 4.24.0. The evalboard features a User Button and the display shield has a joystick-like control element with 5 contacts
The TouchGFX Designer generates a MB1642ButtonController.cpp which has bugs in the getKeyState method.
First failure is to return characters instead of integers, e.g.
keyPressed = '5'
instead of
keyPressed = 5
this fails when compared with
"Key": 5
configured in the .touchgfx file. Because of that no button press is registered.
Second
For the User Button on the evalboard the same method returns 0 (zero).
keyPressed = 0;
But zero is also the default value, so the button press is ignored. Changed it to return 1 and voilà, it works.
The code generated:
"PhysicalButtons": [
{
"Key": 1,
"Name": "BUTTON_USER"
},
{
"Key": 5,
"Name": "BUTTON_CENTER"
}
],uint8_t MB1642ButtonController::getKeyState(void)
{
uint8_t keyPressed = 0;
if (touchgfx::HAL::getInstance()->getDisplayOrientation() == touchgfx::ORIENTATION_PORTRAIT)
{
if (HAL_GPIO_ReadPin(BUTTON_CENTER_GPIO_Port, BUTTON_CENTER_Pin) == GPIO_PIN_RESET)
{
keyPressed = '5'; // Corresponds to keyboard keypad center
}
else if (HAL_GPIO_ReadPin(BUTTON_LEFT_GPIO_Port, BUTTON_LEFT_Pin) == GPIO_PIN_RESET)
{
keyPressed = '4'; // Corresponds to keyboard keypad left
}
else if (HAL_GPIO_ReadPin(BUTTON_RIGHT_GPIO_Port, BUTTON_RIGHT_Pin) == GPIO_PIN_RESET)
{
keyPressed = '6'; // Corresponds to keyboard keypad right
}
else if (HAL_GPIO_ReadPin(BUTTON_UP_GPIO_Port, BUTTON_UP_Pin) == GPIO_PIN_RESET)
{
keyPressed = '8'; // Corresponds to keyboard keypad up
}
else if (HAL_GPIO_ReadPin(BUTTON_DOWN_GPIO_Port, BUTTON_DOWN_Pin) == GPIO_PIN_RESET)
{
keyPressed = '2'; // Corresponds to keyboard keypad down
}
//Blue user button on Nucleo boad
else if (HAL_GPIO_ReadPin(BUTTON_USER_GPIO_Port, BUTTON_USER_Pin) == GPIO_PIN_RESET)
{
keyPressed = '0';
}
}
else
{
if (HAL_GPIO_ReadPin(BUTTON_CENTER_GPIO_Port, BUTTON_CENTER_Pin) == GPIO_PIN_RESET)
{
keyPressed = '5'; // Corresponds to keyboard keypad enter
}
else if (HAL_GPIO_ReadPin(BUTTON_LEFT_GPIO_Port, BUTTON_LEFT_Pin) == GPIO_PIN_RESET)
{
keyPressed = '8'; // Corresponds to keyboard keypad up
}
else if (HAL_GPIO_ReadPin(BUTTON_RIGHT_GPIO_Port, BUTTON_RIGHT_Pin) == GPIO_PIN_RESET)
{
keyPressed = '2'; // Corresponds to keyboard keypad down
}
else if (HAL_GPIO_ReadPin(BUTTON_UP_GPIO_Port, BUTTON_UP_Pin) == GPIO_PIN_RESET)
{
keyPressed = '6'; // Corresponds to keyboard keypad right
}
else if (HAL_GPIO_ReadPin(BUTTON_DOWN_GPIO_Port, BUTTON_DOWN_Pin) == GPIO_PIN_RESET)
{
keyPressed = '4'; // Corresponds to keyboard keypad left
}
//Blue user button on Nucleo boad
else if (HAL_GPIO_ReadPin(BUTTON_USER_GPIO_Port, BUTTON_USER_Pin) == GPIO_PIN_RESET)
{
keyPressed = '0';
}
}
return keyPressed;
}
The fixed code:
uint8_t MB1642ButtonController::getKeyState(void)
{
uint8_t keyPressed = 0;
if (touchgfx::HAL::getInstance()->getDisplayOrientation() == touchgfx::ORIENTATION_PORTRAIT)
{
if (HAL_GPIO_ReadPin(BUTTON_CENTER_GPIO_Port, BUTTON_CENTER_Pin) == GPIO_PIN_RESET)
{
keyPressed = 5; // Corresponds to keyboard keypad center
}
else if (HAL_GPIO_ReadPin(BUTTON_LEFT_GPIO_Port, BUTTON_LEFT_Pin) == GPIO_PIN_RESET)
{
keyPressed = 4; // Corresponds to keyboard keypad left
}
else if (HAL_GPIO_ReadPin(BUTTON_RIGHT_GPIO_Port, BUTTON_RIGHT_Pin) == GPIO_PIN_RESET)
{
keyPressed = 6; // Corresponds to keyboard keypad right
}
else if (HAL_GPIO_ReadPin(BUTTON_UP_GPIO_Port, BUTTON_UP_Pin) == GPIO_PIN_RESET)
{
keyPressed = 8; // Corresponds to keyboard keypad up
}
else if (HAL_GPIO_ReadPin(BUTTON_DOWN_GPIO_Port, BUTTON_DOWN_Pin) == GPIO_PIN_RESET)
{
keyPressed = 2; // Corresponds to keyboard keypad down
}
//Blue user button on Nucleo boad
else if (HAL_GPIO_ReadPin(BUTTON_USER_GPIO_Port, BUTTON_USER_Pin) == GPIO_PIN_RESET)
{
keyPressed = 1;
}
}
else
{
if (HAL_GPIO_ReadPin(BUTTON_CENTER_GPIO_Port, BUTTON_CENTER_Pin) == GPIO_PIN_RESET)
{
keyPressed = 5; // Corresponds to keyboard keypad enter
}
else if (HAL_GPIO_ReadPin(BUTTON_LEFT_GPIO_Port, BUTTON_LEFT_Pin) == GPIO_PIN_RESET)
{
keyPressed = 8; // Corresponds to keyboard keypad up
}
else if (HAL_GPIO_ReadPin(BUTTON_RIGHT_GPIO_Port, BUTTON_RIGHT_Pin) == GPIO_PIN_RESET)
{
keyPressed = 2; // Corresponds to keyboard keypad down
}
else if (HAL_GPIO_ReadPin(BUTTON_UP_GPIO_Port, BUTTON_UP_Pin) == GPIO_PIN_RESET)
{
keyPressed = 6; // Corresponds to keyboard keypad right
}
else if (HAL_GPIO_ReadPin(BUTTON_DOWN_GPIO_Port, BUTTON_DOWN_Pin) == GPIO_PIN_RESET)
{
keyPressed = 4; // Corresponds to keyboard keypad left
}
//Blue user button on Nucleo boad
else if (HAL_GPIO_ReadPin(BUTTON_USER_GPIO_Port, BUTTON_USER_Pin) == GPIO_PIN_RESET)
{
keyPressed = 1;
}
}
return keyPressed;
}