Associate III
February 12, 2025
Question
TouchGFX Frame Buffer: image inverted at corners
- February 12, 2025
- 0 replies
- 521 views
Hi,
I'm facing an issue displaying an image on a 1024x600 screen via RGB. As shown in the image, the frame buffer is displaying part of the image as an inverted image in the corners. I've double-checked the LCD timing parameters, and they all match the datasheet specifications.
I'm using a custom board based on the STM32F429 with external SDRAM.
Please find the attached images for the current configurations.
Your suggestions will be highly appreciated.
Thanks