Associate III
March 4, 2026
Question
Unable to make USB HS Mass storage run with touchgfx
- March 4, 2026
- 0 replies
- 150 views
I have successfully run the USB HS Mass storage on a new project without the use of freertos and touchgfx , But when the touchgfx code for STM32H750B-DK is modified to run the code I am getting hard faults
static uint8_t usb_done = 0;
extern ApplicationTypeDef Appli_state;
extern USBH_HandleTypeDef hUsbHostHS;
extern FATFS USBHFatFS;
extern char USBHPath[4];
void Debug_Print(char *str)
{
HAL_UART_Transmit(&huart4, (uint8_t*)str, strlen(str), 100);
}
static uint8_t file_written = 0;
void StartDefaultTask(void *argument)
{
Debug_Print("Task Started\r\n");
for(;;)
{
USBH_Process(&hUsbHostHS);
if (Appli_state == APPLICATION_READY && file_written == 0)
{
Debug_Print("USB Detected\r\n");
if (USBH_MSC_IsReady(&hUsbHostHS))
{
Debug_Print("MSC Ready\r\n");
FRESULT res;
FIL file;
UINT bw;
/* Mount USB */
Debug_Print("Mounting...\r\n");
res = f_mount(&USBHFatFS, USBHPath, 1);
if (res == FR_OK)
{
Debug_Print("Mount OK\r\n");
/* Create file */
res = f_open(&file,
"0:/log.txt",
FA_CREATE_ALWAYS | FA_WRITE);
if (res == FR_OK)
{
Debug_Print("File Opened\r\n");
char data[] = "Hello from STM32H750 + FreeRTOS\r\n";
res = f_write(&file, data, strlen(data), &bw);
if (res == FR_OK)
Debug_Print("Write OK\r\n");
else
Debug_Print("Write ERROR\r\n");
f_close(&file);
Debug_Print("File Closed\r\n");
}
else
{
Debug_Print("File Open ERROR\r\n");
}
file_written = 1;
}
else
{
Debug_Print("Mount FAILED\r\n");
}
}
}
if (Appli_state == APPLICATION_DISCONNECT)
{
Debug_Print("USB Removed\r\n");
file_written = 0;
}
char msg[50];
sprintf(msg, "State: %d\r\n", hUsbHostHS.gState);
Debug_Print(msg);
}
}I have tried to increase the stack size
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
.name = "defaultTask",
.stack_size = 32768,------>increased
.priority = (osPriority_t) osPriorityNormal,
};
/* Definitions for GUITask */
osThreadId_t GUITaskHandle;
const osThreadAttr_t GUITask_attributes = {
.name = "GUITask",
.stack_size = 8192 * 4,
.priority = (osPriority_t) osPriorityNormal,
};As soon as the mass storage is added the system goes in hardfault
State is printed =1 (serial output)