Senior
December 15, 2025
Solved
Update textArea's wildcard programatically inside keyboard
- December 15, 2025
- 1 reply
- 368 views
Hi again,
I'm looking to implement a character limit on a keyboard, as seen by the red 30/30 text in the screen below.

In CustomKeyboard.hpp I added:
/**
* The buffer used to hold the ASCII representation of the key count (e.g., "5/30").
*/
Unicode::UnicodeChar keyCountTextAreaBuffer[KEYCOUNTTEXTAREA_SIZE];
/**
* Used to display the count of the characters entered / total allowed.
*/
TextAreaWithOneWildcard keyCountTextArea;And in CustomKeyboard.cpp there's some logic to add that textArea to the screen:
CustomKeyboard::CustomKeyboard() : keyboard(),
keyCountTextArea(),
modeBtnTextArea(),
enterBtnTextArea(),
capslockPressed(this, &CustomKeyboard::capslockPressedHandler),
backspacePressed(this, &CustomKeyboard::backspacePressedHandler),
modePressed(this, &CustomKeyboard::modePressedHandler),
enterPressed(this, &CustomKeyboard::enterPressedHandler),
keyPressed(this, &CustomKeyboard::keyPressedHandler),
alphaKeys(true),
uppercaseKeys(false),
firstCharacterEntry(false)
{
alphaLayout.callbackAreaArray[0].callback = &capslockPressed;
alphaLayout.callbackAreaArray[1].callback = &backspacePressed;
alphaLayout.callbackAreaArray[2].callback = &modePressed;
alphaLayout.callbackAreaArray[3].callback = &enterPressed;
numLayout.callbackAreaArray[0].callback = &backspacePressed;
numLayout.callbackAreaArray[1].callback = &modePressed;
numLayout.callbackAreaArray[2].callback = &enterPressed;
keyboard.setLayout(&alphaLayout);
keyboard.setKeyListener(keyPressed);
keyboard.setPosition(0, 0, 480, 320);
keyboard.setTextIndentation();
memset(buffer, 0, sizeof(buffer));
keyboard.setBuffer(buffer, BUFFER_SIZE);
uppercaseKeys = true;
firstCharacterEntry = true;
keyCountTextArea.setPosition(FIRST_ROW_X + 386, ZEROETH_ROW_Y, ENTER_MODE_WIDTH, KEY_HEIGHT);
keyCountTextArea.setColor(Color::getColorFromRGB(0xFF, 0xFF, 0xFF));
modeBtnTextArea.setPosition(FIRST_ROW_X, FOURTH_ROW_Y + 8, ENTER_MODE_WIDTH, KEY_HEIGHT);
modeBtnTextArea.setColor(Color::getColorFromRGB(0xFF, 0xFF, 0xFF));
enterBtnTextArea.setPosition(ENTER_X, FOURTH_ROW_Y + 8, ENTER_MODE_WIDTH, KEY_HEIGHT);
enterBtnTextArea.setColor(Color::getColorFromRGB(0xFF, 0xFF, 0xFF));
enterBtnTextArea.setTypedText(TypedText(T_ENTER));
setKeyMappingList();
add(keyboard);
add(keyCountTextArea);
add(modeBtnTextArea);
add(enterBtnTextArea);
}And then I have the following function which implements the logic for key counting:
void CustomKeyboard::updateKeyCount()
{
int keyCount = keyboard.getBufferPosition();
Unicode::snprintf(keyCountTextAreaBuffer, sizeof(keyCountTextAreaBuffer), "%u/%u", keyCount, BUFFER_SIZE - 1);
if (keyCount >= BUFFER_SIZE - 1)
{
keyCountTextArea.setColor(Color::getColorFromRGB(0xFF, 0x00, 0x00));
}
else
{
keyCountTextArea.setColor(Color::getColorFromRGB(0xFF, 0xFF, 0xFF));
}
keyCountTextArea.setWildcard(keyCountTextAreaBuffer);
keyCountTextArea.invalidate();
}I call this function from `keyPressedHandler` and `backspacePressedHandler`, however I never see the text appear.
I tried adding some logic that conditionally determines which TypedText to display in the textArea, and that works fine.
void CustomKeyboard::updateKeyCount()
{
int keyCount = keyboard.getBufferPosition();
if (keyCount >= BUFFER_SIZE - 1)
{
keyCountTextArea.setTypedText(TypedText(T_HITLIMIT));
}
else
{
keyCountTextArea.setTypedText(TypedText(T_ALLGOOD));
}
keyCountTextArea.invalidate();
}
I must be doing something silly with wildcards! Any help is appreciated, thank you,
Julia