Using an existing DK TouchGFXDesigner Demo project on a custom board
I've been working on a board bring up of a STM32U5G7 for a few days following https://support.touchgfx.com/docs/development/board-bring-up/board-introduction
While the board is able to display the framebuffer and change colours, etc, when I finally complete the bring up process to include TouchGFX generation and TouchGFXDesigner, the project does not run out of the box and it's difficult to debug and tell what's missing.
Instead, since the demos and examples from the STM32U5G9J-DK2 easily compile/run and that there are only a few differences between my board and the kit, would it be possible to modify/copy a DK based application to run on my board?
The differences are:
- MCU package U5G9 144pin vs U5G7 100pin
- external flash not used
I'd be happy to make sure the MCU pins are used correct and clock config, etc. but this way at least I know I'm not missing anything.