Using USB PD and TouchGFX Together on STM32U575
Hi Everyone,
I’m working with an STM32U575 and facing an issue when trying to use USB-PD (X-CUBE-TCPP) together with TouchGFX.
In CubeMX, it does not allow enabling both X-CUBE-TCPP (USB-PD) and TouchGFX Generator at the same time. It shows a restriction that only one application can be selected.
We are trying to implement USPD along with touchGFX on STM32U5757. We have implemented induvial and tested both are working well. But when we trying to merge them, then both are not running . We have seen in cubeMX that is not allow us to select both at same time, it says you can't use both at same time. Then we read the st community and found we can merge them manually . We tried to merge but after initialization of one other one hangs. Can you clear that is it possible to use both at same time in U575 MCU?
Note- we are using free RTOS
Thanks & Regards,
Rajkumar