What is the cause of the screen shift?
Hi All,
Im working with a Custom board using STM32h743 and an RGB Display with ST7796 driver.
I'm configuring SPI to send the right settings to the display for working with RGB pins on LTDC.
In effect I done the 90% of work but I don't understand the reason of the effect on the below image:

Display draw the screen with wrong pixels: it seems shifted.
The original screen created with TouchGFX Designer is:

Whitch parameter is the cause of this effect?
Does someone has some suggestions?
Thanks a lot?