Skip to main content
JPabl.1
Associate III
October 16, 2024
Solved

Widgets are redrawn after invalidate, how not to?

  • October 16, 2024
  • 2 replies
  • 756 views

Hi there Touchgfx team!

 

I have these screens

JPabl1_0-1729084934253.png

I already implemented all the navigation. When I'm in volume screen, if I start pressing the up/down arrow buttons, the read widgets appears again. Is there any way to avoid this different than calling invalidate() every single time? 

All those 4 screens are developed inside a single screen. Based on the user input, I just change their state to visible/invisible. 

Thanks a lot in advance

Best answer by Mohammad MORADI ESFAHANIASL

Hello @JPabl.1,

As you mentioned, you just need to change the visibility state of the READ widget. There should be a misconfiguration in your logic that causes the READ widget appear if the up/down buttons are pressed. You can also call invalidate() only for the widgets you are changing (instead of the whole screen, which can save a lot of unnecessary calculations).

So please, ensure you are using SetVisible(bool visibility) in the correct order. If you still have issues, please share the part of your code that is causing the issue. 

I hope this helps you!

 

2 replies

ST Employee
October 16, 2024

Hello @JPabl.1,

As you mentioned, you just need to change the visibility state of the READ widget. There should be a misconfiguration in your logic that causes the READ widget appear if the up/down buttons are pressed. You can also call invalidate() only for the widgets you are changing (instead of the whole screen, which can save a lot of unnecessary calculations).

So please, ensure you are using SetVisible(bool visibility) in the correct order. If you still have issues, please share the part of your code that is causing the issue. 

I hope this helps you!

 

JPabl.1
JPabl.1Author
Associate III
October 16, 2024

I missed a invalidate() call, thanks

ST Employee
October 17, 2024

Glad to hear you have fixed it :D

You're very welcome!

Best regards,