aci_hal_set_event_mask and ACI_HAL_SCAN_REQ_REPORT_VSEVT_CODE
There are already a few threads discussing this topic, but none of them have an answer.
How can one force the STM32WB35 to send an event upon receiving a scan request? The documentation (rather vaguely) states that this can be achieved by setting the appropriate mask (0x1u) when calling the aci_hal_set_event_mask function (as far as I remember, there is no mention anywhere that this function is available only in BLE_Stack_full_extended_fw.bin).
Even though the function executes successfully (returns 0), during scanning (with NRFConnect) I do not receive any information from the stack indicating that someone has read the data from the scan response.
In SVCCTL_App_Notification, I am handling HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE, and within that, I handle ACI_HAL_SCAN_REQ_REPORT_VSEVT_CODE.
Best,
msemegen