AN2606 Rev 69 - STM32WBA6x: USART2 vs USART3 discrepancy in bootloader section
In AN2606 Rev 69, the STM32WBA6x system bootloader section describes the UART interface as USART3, but there appear to be errors:
1. Inconsistency within the same entry:
The TX pin description mixes USART2 and USART3 in the same sentence:
USART3_TX pin Output PA12 pin: USART2 in transmission mode. Kept in reset configuration until 0x7F detected on USART_RX.
While the RX pin description correctly uses USART3:
USART3_RX pin Input PA11 pin: USART3 in reception mode. Used in alternate push-pull, pull-up mode.
2. PA11/PA12 are assigned to USART2, not USART3:
According to the STM32WBA62 datasheet, PA11 and PA12 are mapped to USART2 (USART2_RX / USART2_TX), not USART3.
Question:
Does the STM32WBA6x system bootloader actually use USART2 on PA11/PA12? It seems the document should read USART2 throughout, and the current "USART3" label is an error.
Could ST please clarify and correct this in the next revision of AN2606?
Environment:
- Document: AN2606 Rev 69
- MCU: STM32WBA62CGU6
- Section: STM32WBA6x bootloader - USART