B-WB1M-WPAN1
Colleagues,
I need to implement the BLE_CableReplacement project on the b_wb1m_wpan1 device. Since I don’t know the services of this project (the BLE_CableReplacement.ioc file is not included), I tried to adapt the project for the b_wb1m_wpan1 device in IAR.
Steps I took:
In IAR General Options, selected ST STM32WB1MMC.
Copied the B-WB1M-WPAN1 folder into the BSP directory of the BLE_CableReplacement project.
Added a reference in the preprocessor options.
Removed stm32wbxx_nucleo.c from the project tree.
Replaced it with b_wb1m_wpan1.c and commented out all instances of //#include "stm32wbxx_nucleo.h".
Opened the standard set of files:
stm32wb55xx_flash_cm4.icf
startup_stm32wb55xx_cm4.s
system_stm32wbxx.c
Replaced their contents via clipboard with the corresponding files from the BLE_HR_p2p_Sensor project.
The system prompted me to copy b_wb1m_wpan1_conf.h into the Core → Inc directory. I did so.
Replaced all instances of DMA2_Channel4 with DMA1_Channel5.
After these changes, the project compiles but gets stuck at the MX_APPE_Process() function and shows no further signs of life.
Could you please advise:
What did I miss?
What would be a better approach?