Skip to main content
Associate III
February 13, 2024
Question

BLE Always Fails when setting RFWKP Clock Mux to LSE

  • February 13, 2024
  • 5 replies
  • 3363 views

I've been having a lot of trouble getting all of the online BLE examples to work and was hoping someone could steer me in the right direction.  In every example they state that the RFWKP Clock Mux should be set to LSE but whenever I do that the main loops runs once then hangs somewhere in MX_APPE_Process() but I'm not sure where.  Interestingly if I setup a timer and ADC (to give it something else to do) that part works just fine - my ADC loop just reads a few values every second then toggles and LED.  

If I set the RFWKP Clock to HSE then it seems to work fine.  

I thought it was a problem with my custom board but this happens with the P-NUCLEO-WB55 board as well.

I'm using STM32CubeIDE version 1.14.1 and have the latest version of the FUS and wireless stack installed.  

5 replies

STTwo-32
Technical Moderator
February 13, 2024

Hello @nollstead 

I've tested personally with different examples ( Ble_HealthThermometer for example). Those examples are all using the HSE as a source clock for the RFWKP Clock. Everything works fine for me.

Can you give more details about the example you are using.

Best Regards.

STTwo-32

nollsteadAuthor
Associate III
February 13, 2024

I'm basically following the tutorial at https://www.youtube.com/watch?v=Zgw3wRpGSRQ 

The only difference is that I'm also adding in some ADC code that's based on a timer - so instead of reading a button the plan is to send it data that comes from and ADC/Timer/DMA source.  I had the same issue without the ADC part so that's not the problem.

In my current code all I'm doing is the ADC stuff and broadcasting two read/notify attributes (that aren't hooked up to events yet).  In the ADC callback I'm flashing the blue light and in main I'm alternating the red and green lights

Below is my clock configuration.  With RFWKP set to LSE the blue light flashes as expected (indicating that the ADC timer is firing) but the red and green lights come on and stay on (indicating that the while only runs once) and no BLE is advertised.  The lights are an easy indication but I can confirm via the debugger that the main while loop only runs once.  If I just change the RFWKP to HSE then everything works fine (blue light flashes, red/green alternate and I can connect to the BLE service)

 

4d2f8f7f-692e-4161-bad4-887465d2a596.png

 

Here is my main.c code as that's the only file I changed myself (though STM32CubeIDE made it's own changes to other files for RF, etc.).  I'm not sure if there are other files or settings you'd like to see or if it would be easier if I just uploaded a zip of the whole project.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.

 * Notes:
 * 1. Timer calculator: https://deepbluembedded.com/stm32-timer-calculator/
 * 2.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
//#include "stm32_seq.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

IPCC_HandleTypeDef hipcc;

RTC_HandleTypeDef hrtc;

TIM_HandleTypeDef htim2;

/* USER CODE BEGIN PV */
uint32_t AD_RES_BUFFER[2];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_RTC_Init(void);
static void MX_TIM2_Init(void);
static void MX_ADC1_Init(void);
static void MX_IPCC_Init(void);
static void MX_RF_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {

	uint8_t JoyX, JoyY;

	// Just read for now, later I'll add to variables to be exposed to the BLE services
	JoyX = AD_RES_BUFFER[0];
	JoyY = AD_RES_BUFFER[1];
	HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin);
}

void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef *hadc) {
	uint8_t x = 0;

	// Just a place to stick a breakpoint later for testing
	x++;

}


/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 uint8_t bufLen;
 char txBuf[128];


 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */
 MX_APPE_Config();

 /* USER CODE BEGIN Init */
 //LL_HSEM_1StepLock( HSEM, 5 ); // CES: Forum has this as a fix for USB+BLE

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

/* Configure the peripherals common clocks */
 PeriphCommonClock_Config();

 /* IPCC initialisation */
 MX_IPCC_Init();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RTC_Init();
 MX_TIM2_Init();
 MX_ADC1_Init();
 MX_RF_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);
 HAL_TIM_Base_Start(&htim2);
 HAL_ADC_Start_DMA(&hadc1, (uint32_t *) AD_RES_BUFFER, 2);

 /* USER CODE END 2 */

 /* Init code for STM32_WPAN */
 MX_APPE_Init();

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 //HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin);
	 //HAL_Delay(1000);
		//bufLen = snprintf(txBuf, 512, "J2PotX: %u\tJ2PotY: %u\r\n",data.j2PotX, data.j2PotY);
	 //bufLen = snprintf(txBuf, 128, "%s", "This is a test\r\n");
	 //CDC_Transmit_FS((uint8_t *) txBuf, bufLen);
	 HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
	 HAL_Delay(500);
	 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
	 HAL_Delay(500);

 /* USER CODE END WHILE */
 MX_APPE_Process();

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
 |RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
 |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_RFWAKEUP;
 PeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_LSE;
 PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSE;
 PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN Smps */

 /* USER CODE END Smps */
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_8B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_640CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief IPCC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_IPCC_Init(void)
{

 /* USER CODE BEGIN IPCC_Init 0 */

 /* USER CODE END IPCC_Init 0 */

 /* USER CODE BEGIN IPCC_Init 1 */

 /* USER CODE END IPCC_Init 1 */
 hipcc.Instance = IPCC;
 if (HAL_IPCC_Init(&hipcc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN IPCC_Init 2 */

 /* USER CODE END IPCC_Init 2 */

}

/**
 * @brief RF Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_RF_Init(void)
{

 /* USER CODE BEGIN RF_Init 0 */

 /* USER CODE END RF_Init 0 */

 /* USER CODE BEGIN RF_Init 1 */

 /* USER CODE END RF_Init 1 */
 /* USER CODE BEGIN RF_Init 2 */

 /* USER CODE END RF_Init 2 */

}

/**
 * @brief RTC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_RTC_Init(void)
{

 /* USER CODE BEGIN RTC_Init 0 */

 /* USER CODE END RTC_Init 0 */

 /* USER CODE BEGIN RTC_Init 1 */

 /* USER CODE END RTC_Init 1 */

 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = CFG_RTC_ASYNCH_PRESCALER;
 hrtc.Init.SynchPrediv = CFG_RTC_SYNCH_PRESCALER;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable the WakeUp
 */
 if (HAL_RTCEx_SetWakeUpTimer(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */

 /* USER CODE END RTC_Init 2 */

}

/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 49999;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 127;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LD2_Pin|LD3_Pin|LD1_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : D7_Pin B1_Pin D2_Pin D4_Pin
 D8_Pin */
 GPIO_InitStruct.Pin = D7_Pin|B1_Pin|D2_Pin|D4_Pin
 |D8_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pins : PWM_D6_Pin PWMD3_Pin PWM_D5_Pin */
 GPIO_InitStruct.Pin = PWM_D6_Pin|PWMD3_Pin|PWM_D5_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : LD2_Pin LD3_Pin LD1_Pin */
 GPIO_InitStruct.Pin = LD2_Pin|LD3_Pin|LD1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : B2_Pin B3_Pin */
 GPIO_InitStruct.Pin = B2_Pin|B3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : STLINK_RX_Pin STLINK_TX_Pin */
 GPIO_InitStruct.Pin = STLINK_RX_Pin|STLINK_TX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

nollsteadAuthor
Associate III
February 15, 2024

@STTwo-32 I've done a bit more testing and have more information.

 

1.  As before, when I change RFWKP to LSE it only executes the while once but runs as normal when set to HSE.  Note that this is a custom BLE, not one of the pre-built ones.

2.  I went in and added the additional code from the part 12c video (the sequencer code) and again BLE halts and the main wait only executes once.  This happens when I register my task (myBLENotifyTask) with the sequencer.  If I comment out those two lines in the user code section it works fine:

void APP_BLE_Init(void)
{
 SHCI_CmdStatus_t status;
#if (RADIO_ACTIVITY_EVENT != 0)
 tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
#endif /* RADIO_ACTIVITY_EVENT != 0 */
 /* USER CODE BEGIN APP_BLE_Init_1 */
 UTIL_SEQ_RegTask(1 << CFG_TASK_MY_BLE_NOTIFY_TASK, UTIL_SEQ_RFU, myBLENotifyTask);
 UTIL_SEQ_SetTask(1 << CFG_TASK_MY_BLE_NOTIFY_TASK, CFG_SCH_PRIO_0);

3.  I used CubeIDE to create a new custom BLE app from the example selector and it had the same behavior.  The code is structured very differently and I haven't found how to test commenting out the sequencer task registration yet but as it was created it halts in while and doesn't run the BLE apps.

So while I'm not sure if the first issue is related (LSE vs. HSE) the second two suggest there is some sort of issue with the sequencer.  

nollsteadAuthor
Associate III
February 15, 2024

Ignore my last comment.  I reflashed both the FUS and BLE stack and the latest problem went away.  Not sure why I had to do that but I've seen a lot of folks mention it in comments so it was worth a shot - a bit concerning but we'll see how that goes.

 

I'm back to the original problem.  When any app runs with RFWKP clock set to LSE it doesn't work.  When set to HSE it works.

STTwo-32
Technical Moderator
February 16, 2024

Hello again @nollstead 

I can't reproduce this issue. We have a lot of examples that use the LSE as clock source for the RFWKP and everything works fine.

Can you share your project for more details.

Best Regards.

STTwo-32 

nollsteadAuthor
Associate III
February 16, 2024

Sure, attached is a rar archive of a project called Nucleo-WB55.  If there is a different format you need let me know (zip uploads aren't permitted so I used rar).  

All it does it grab a few variables via an ADC timer and blink a few lights in that event and in main and exposes a BLE service with 1 characteristic (which I don't do anything with yet).  

As uploaded the RFWKP clock is set to LSE and nothing is advertised in BLE.  Setting a breakpoint on the call to MX_APPE_Process shows it only runs once (also confirmed by the green light staying on). 

If I just change the RFWKP clock to HSE it works (BLE device called "NUCLEO-WB55 shows up and is connectable and the green light flashes.

 

nollsteadAuthor
Associate III
February 17, 2024

@STTwo-32 I've created a new project and (painstakingly) added each feature one by one and now know what causes this behavior - I'm just not sure why or what to do about it.

 

As I mentioned in my original post, this is a remote control - so it uses a timer to poll the components every 200ms and exposes a BLE service to advertise those.  Each part works fine on its own but when put together I get the issue where the main loop only executes once (and BLE doesn't advertise).  

I've narrowed it down to the ADC/Timer combination. That would probably explain why STM's examples that use LSE work - I don't think any of them combine with a timer driving ADC with BLE.

 

  • When the ADC External Trigger Conversion Source is set to "Regular Conversion Launched by Software" then I can use LSE as the RFWKP clock and BLE is advertised (obviously I don't get any ADC conversions though).
  • When the ADC External Trigger Conversion Source is set to "Timer 2 Trigger Out Event" I have to switch the RFWKP clock to HSE.  It's this combination that causes the problem.

Is this normal?  

 

Below is my main.c that exhibits the problem - which I think has all of the timer and ADC related code though I can upload the entire project again if you need that.  Again, if I either change to software triggered ADC OR switch clock to HSE then it seems to work fine - I just can't do both:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

IPCC_HandleTypeDef hipcc;

RTC_HandleTypeDef hrtc;

TIM_HandleTypeDef htim2;

/* USER CODE BEGIN PV */
volatile uint32_t AD_RES_BUFFER[2];
volatile uint8_t j1PotX;
volatile uint8_t j1PotY;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_RTC_Init(void);
static void MX_ADC1_Init(void);
static void MX_TIM2_Init(void);
static void MX_IPCC_Init(void);
static void MX_RF_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {
	j1PotX = AD_RES_BUFFER[0];
	j1PotY = AD_RES_BUFFER[1];


	// Continuous ADC conversion of Analog inputs is complete and stored in the data structure to be used later.
	//data.j1PotX = (uint8_t) MAP(AD_RES_BUFFER[0], 0, 4096, 0, 256);
	//data.j1PotY= (uint8_t) MAP(AD_RES_BUFFER[1], 0, 4096, 0, 256);
	//data.j2PotX = (uint8_t) MAP(AD_RES_BUFFER[2], 0, 4096, 0, 256);
	//data.j2PotY = (uint8_t) MAP(AD_RES_BUFFER[3], 0, 4096, 0, 256);
	//data.pot1 = (uint8_t) MAP(AD_RES_BUFFER[4], 0, 4096, 0, 256);
	//data.pot2 = (uint8_t) MAP(AD_RES_BUFFER[5], 0, 4096, 0, 256);
	//data.BatteryVoltage = AD_RES_BUFFER[6];

	// For convenience, read digital pins here
	//data.j1Button = HAL_GPIO_ReadPin(j1Button_GPIO_Port, j1Button_Pin);
	//data.j2Button = HAL_GPIO_ReadPin(j2Button_GPIO_Port, j2Button_Pin);
	//data.tSwitch1 = HAL_GPIO_ReadPin(tSwitch1_GPIO_Port, tSwitch1_Pin);
	//data.tSwitch2 = HAL_GPIO_ReadPin(tSwitch2_GPIO_Port, tSwitch2_Pin);
	//data.button1 = HAL_GPIO_ReadPin(Button1_GPIO_Port, Button1_Pin);
	//data.button2 = HAL_GPIO_ReadPin(Button2_GPIO_Port, Button2_Pin);
	//data.button3 = HAL_GPIO_ReadPin(Button3_GPIO_Port, Button3_Pin);
	//data.button4 = HAL_GPIO_ReadPin(Button4_BOOT0_GPIO_Port, Button4_BOOT0_Pin);

	HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);

}

uint16_t MAP(uint16_t au16_IN, uint16_t au16_INmin, uint16_t au16_INmax, uint16_t au16_OUTmin, uint16_t au16_OUTmax)
{
 return ((((au16_IN - au16_INmin)*(au16_OUTmax - au16_OUTmin))/(au16_INmax - au16_INmin)) + au16_OUTmin);
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */
 MX_APPE_Config();

 /* USER CODE BEGIN Init */
 LL_HSEM_1StepLock( HSEM, 5 ); // CES: Forum has this as a fix for USB+BLE

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

/* Configure the peripherals common clocks */
 PeriphCommonClock_Config();

 /* IPCC initialisation */
 MX_IPCC_Init();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_RTC_Init();
 MX_ADC1_Init();
 MX_TIM2_Init();
 MX_USB_Device_Init();
 MX_RF_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);
 // Turn on Blue LED, indicating that we're NOT in boot mode and all initializations are complete
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_SET);
 HAL_TIM_Base_Start(&htim2);
 HAL_ADC_Start_DMA(&hadc1, (uint32_t *) AD_RES_BUFFER, 2);

 /* USER CODE END 2 */

 /* Init code for STM32_WPAN */
 MX_APPE_Init();

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 MX_APPE_Process();

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Macro to configure the PLL multiplication factor
 */
 __HAL_RCC_PLL_PLLM_CONFIG(RCC_PLLM_DIV2);

 /** Macro to configure the PLL clock source
 */
 __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
 |RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
 |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_RFWAKEUP
 |RCC_PERIPHCLK_USB|RCC_PERIPHCLK_ADC;
 PeriphClkInitStruct.PLLSAI1.PLLN = 6;
 PeriphClkInitStruct.PLLSAI1.PLLP = RCC_PLLP_DIV2;
 PeriphClkInitStruct.PLLSAI1.PLLQ = RCC_PLLQ_DIV2;
 PeriphClkInitStruct.PLLSAI1.PLLR = RCC_PLLR_DIV2;
 PeriphClkInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_USBCLK|RCC_PLLSAI1_ADCCLK;
 PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLLSAI1;
 PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLLSAI1;
 PeriphClkInitStruct.RFWakeUpClockSelection = RCC_RFWKPCLKSOURCE_LSE;
 PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSE;
 PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN Smps */

 /* USER CODE END Smps */
}

/**
 * @brief ADC1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_8B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_15;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_640CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_16;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief IPCC Initialization Function
 * @param None
 * @retval None
 */
static void MX_IPCC_Init(void)
{

 /* USER CODE BEGIN IPCC_Init 0 */

 /* USER CODE END IPCC_Init 0 */

 /* USER CODE BEGIN IPCC_Init 1 */

 /* USER CODE END IPCC_Init 1 */
 hipcc.Instance = IPCC;
 if (HAL_IPCC_Init(&hipcc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN IPCC_Init 2 */

 /* USER CODE END IPCC_Init 2 */

}

/**
 * @brief RF Initialization Function
 * @param None
 * @retval None
 */
static void MX_RF_Init(void)
{

 /* USER CODE BEGIN RF_Init 0 */

 /* USER CODE END RF_Init 0 */

 /* USER CODE BEGIN RF_Init 1 */

 /* USER CODE END RF_Init 1 */
 /* USER CODE BEGIN RF_Init 2 */

 /* USER CODE END RF_Init 2 */

}

/**
 * @brief RTC Initialization Function
 * @param None
 * @retval None
 */
static void MX_RTC_Init(void)
{

 /* USER CODE BEGIN RTC_Init 0 */

 /* USER CODE END RTC_Init 0 */

 /* USER CODE BEGIN RTC_Init 1 */

 /* USER CODE END RTC_Init 1 */

 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = CFG_RTC_ASYNCH_PRESCALER;
 hrtc.Init.SynchPrediv = CFG_RTC_SYNCH_PRESCALER;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable the WakeUp
 */
 if (HAL_RTCEx_SetWakeUpTimer(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */

 /* USER CODE END RTC_Init 2 */

}

/**
 * @brief TIM2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 127;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 49999;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : Button4_BOOT0_Pin */
 GPIO_InitStruct.Pin = Button4_BOOT0_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 HAL_GPIO_Init(Button4_BOOT0_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : j2Button_Pin */
 GPIO_InitStruct.Pin = j2Button_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(j2Button_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : tSwitch2_Pin tSwitch1_Pin */
 GPIO_InitStruct.Pin = tSwitch2_Pin|tSwitch1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : Button1_Pin Button3_Pin */
 GPIO_InitStruct.Pin = Button1_Pin|Button3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : j1Button_Pin */
 GPIO_InitStruct.Pin = j1Button_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(j1Button_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : Button2_Pin */
 GPIO_InitStruct.Pin = Button2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 HAL_GPIO_Init(Button2_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : LED_Pin */
 GPIO_InitStruct.Pin = LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

STTwo-32
Technical Moderator
February 20, 2024

Hello @nollstead 

Could you share the project so we can investigate on it. 

Best regards.

STTwo-32

nollsteadAuthor
Associate III
February 20, 2024

Thanks @STTwo-32 ,

 

On the 16th I uploaded a basic nucleo-wb55 version that demonstrated the ADC/Timer/RF issue above.  Attached here is the current project.  This one uses an WB55CGU6 MCU but has the same issues - so two different projects, two different boards, same 2 issues.

 

1.  The issue above (ADC/Timer/RF) - can't use Timer 2 Trigger Out Event and LSE together.

2. If I just leave it set to HSE and keep going then it's fine UNTIL I register my task in the sequencer.  Once I do that the BLE and ADC/Timer works but I again only hit main once.  It seems to go into the sequencer and never return to main.

 

 

STTwo-32
Technical Moderator
April 8, 2024

Hello @nollstead 

Sorry for may late replay. Can you give more details about the configuration you are using and add a simple project that will help to reproduce the issue. I personally can't reproduce this issue. 

Best Regards.

STTwo-32

Visitor II
October 11, 2024

I have the same problem when run the examples on P-NUCLEO-WB55 MB1355-D01, such as BLE_HeartRate and BLE_p2pServer in STM32Cube\Repository\STM32Cube_FW_WB_V1.16.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE.

MrY_1-1728637544069.png

 

MrY_0-1728637500392.png

I have confirmed that LSE was ready by lSCO pin. After modifing the code ccording to the picture above, both BLE_p2pServer and BLE_HeartRate can work.

 

Visitor II
October 11, 2024

Here is the stack when using the LSE as a source clock for the RFWKP Clock.

MrY_0-1728639401536.png

It trapped in while loop:

MrY_1-1728639861907.png