BLE_AT_CLIENT on B-U585-IOT02A – AT+BLE_SVC=1 does not appear despite WB5M update
- November 24, 2025
- 0 replies
- 97 views
Hello everyone,
I am currently working with the BLE_AT_CLIENT example on the B-U585-IOT02A and have previously updated the integrated STM32WB5M according to the instructions in readme.md. The start screen of the example appears correctly (screenshot: BLE.png).
However, a problem occurs which, according to this article https://mind.be/blog/using-the-bluetooth-stack-on-the-b-u585i-iot02a-board/ should occur immediately at start-up and independently of a BLE connection:
The command TX: AT+BLE_SVC=1 does not appear for me.
Normally, this command should be sent automatically immediately after TX: AT. However, only TX: AT is displayed on my device, and then nothing else happens.
Question for the community:
Is anyone familiar with this behaviour or know what could be causing the example to stop at initialisation and prevent AT+BLE_SVC=1 from being sent in the first place?
I would be very grateful for any tips on diagnosis or possible pitfalls.
Many thanks!