BLE-HID demo of STM32Cube_FW_WB_V1.14.1 not working with Android 12 and 13 ?
BLE-HID demo of STM32Cube_FW_WB_V1.14.1 not working with Android 13 ?
Hello,
The BLE_Hid of demo STM32Cube_FW_WB_V1.14.1 does not work with my Android 13 phone at all (services cannot be listed at all in nRFconnect)
while it only kind of works with my Android 12 one (I can list the services with nRFconnect but cannot access them with an error BLUETOOTH_PRIVILEDGED required).
- STM32CubeIDE Version: 1.12.0 Build: 14980_20230301_1550 (UTC)
- STM32Cube_FW_WB_V1.14.1
- BLE stack used is stm32wb5x_BLE_Stack_light_fw.bin from the same firmware package, and I have confirmed that it works using other example projects (BLE_Beacon for example)
- code is STM32Cube_FW_WB_V1.14.1\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_Hid without any modification
- Nucleo board has no modification, and has the appropriate jumpers (tested using other BLE demos)
The serial interface of the HID demo (the menu allowing to select mouse x,y,wheel and buttons) works as expected when clicking SW1, and I can change the values in that menu.
With both phones, I can connect to the device using BLE, and bond it using the 111111 key.
HOWEVER:
When using a Samsung Galaxy S22 with Android 13, if I connect to the device using nRFConnect, the services list just never loads.
With everything else identical but on a Pixel 3a running Andoird 12, nRFconnect can list the services, but cannot access any data with the error "BLUETOOTH_PRIVILEDGED required".
Can anyone confirm what I am seeing? Is there a known fix to run this demo on Android 12 and 13 ?
Best regards,
Nicolas