Skip to main content
Remi Demers
Associate II
April 1, 2025
Solved

BLUENRG-LPS flashing problem

  • April 1, 2025
  • 1 reply
  • 396 views

Hi,

I am starting to work with STEVAL-IDB012V1A. I use Wise-studio version: 1.3.1_R on Linux. I can compile successfully the example "Profiles_Peripheral_with_Library". In the launch configuration I selected CMSIS-DAP. I do hold PUSH1 button while pressing reset before launching the programming. When I click the green arrow to program I get this in the console:

Open On-Chip Debugger 0.12.0-rc2+dev-00962-g12ce17094-dirty (2022-11-07-16:26)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "swd". To override use 'transport select <transport>'.
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: FW Version = 0254
Info : CMSIS-DAP: Serial# = 0720000197969908a5a5a5a505d5ff383650503043146928
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 1200 kHz
Info : SWD DPIDR 0x0bc11477
Info : [bluenrg-lps.cpu] Cortex-M0+ r0p1 processor detected
Info : [bluenrg-lps.cpu] target has 4 breakpoints, 2 watchpoints
Info : starting gdb server for bluenrg-lps.cpu on 3333
Info : Listening on port 3333 for gdb connections
[bluenrg-lps.cpu] halted due to debug-request, current mode: Thread
xPSR: 0xf1000000 pc: 0x100017e8 msp: 0x20005ff8
** Programming Started **
Info : Padding image section 0 at 0x1005eb9c with 4 bytes (bank write end alignment)
Warn : Adding extra erase range, 0x1005eba0 .. 0x1005efff
Error: CMSIS-DAP transfer count mismatch: expected 12, got 4
Info : SWD DPIDR 0x0bc11477
Error: Failed to write memory at 0x20004214
Error: error writing to flash at address 0x10040000 at offset 0x00000000
** Programming Failed **
shutdown command invoked

Warn : Flash driver of bluenrg-lps.flash does not support free_driver_priv()

 

The addresses where the memory write failed are not the same every time. I got it programmed successfully a few times before but now it always fail. Any clue to get out of this?

Thanks,

Rémi

Best answer by Remi Demers

I found the problem. My USB hub had not enough power. Connected directly to the computer it works.

1 reply

Remi Demers
Remi DemersAuthorBest answer
Associate II
April 1, 2025

I found the problem. My USB hub had not enough power. Connected directly to the computer it works.